8GB DDR3 interfacing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

8GB DDR3 interfacing

Jump to solution
1,069 Views
qammarabbas
Contributor IV

Hi,
I am trying to interface 8GB DDR3L RAM with T1042. How can i achieve it? Maximum size of a DDR3L RAM chip is 1GB and the reference manual of T1042 clearly mentions that there are only 4 chip selects available. Consequently, i can only interface 4GB (4*1GB) RAM with it. But i've seen some boards where T1042 is interfaced with a 8GB RAM. Please guide me if i am doing something wrong. Thank you!

1 Solution
786 Views
ufedor
NXP Employee
NXP Employee

Your understanding is correct.

View solution in original post

10 Replies
786 Views
ufedor
NXP Employee
NXP Employee

Note that the T1042 DDR controller supports 64-bit-wide bus.

Please refer to the QorIQ T1040 Reference Manual, 14.5.1.1 Supported DDR SDRAM Organizations.

0 Kudos
786 Views
qammarabbas
Contributor IV

Yes, i have seen this. But how can i interface 8GB RAM with T1042? 

0 Kudos
786 Views
ufedor
NXP Employee
NXP Employee

What exactly is not clear?

2017-11-03_143820.jpg

786 Views
qammarabbas
Contributor IV

Well i am confused between the two terms "bank" and "chip". What does a chip mean? Does it mean a single SDRAM chip (SDRAM Device in the table) or does it mean a bank which can support many chips?

0 Kudos
786 Views
ufedor
NXP Employee
NXP Employee

> What does a chip mean? Does it mean a single SDRAM chip

Chip = single SDRAM device

0 Kudos
786 Views
qammarabbas
Contributor IV

If that is the case then we have 4 chip selects available and the maximum size of 1 chip can be 1GB according to this table. using all 4 chip selects will then give me 4GB maximum (4*1GB). How can i get 8GB?

0 Kudos
786 Views
ufedor
NXP Employee
NXP Employee

Please read the processor's RM and and consider that the table in question shows data for the 64-bit SDRAM bank.

It is obvious that several SDRAM chips must be used to form 64-bit memory bank - examples:

16-bit chip x 4

8-bit chip x 8

0 Kudos
786 Views
qammarabbas
Contributor IV

Thank you!
Please correct me if i am wrong. For a single bank of 64 bits, if i am using 8bit SDRAM devices to build this 64 bit bank then i'll be using 8 SDRAM devices. So, all those 8 SDRAM devices will be given 1 chip select (suppose MCS0_B)?

0 Kudos
787 Views
ufedor
NXP Employee
NXP Employee

Your understanding is correct.

786 Views
qammarabbas
Contributor IV

Thanks a lot ufedor

0 Kudos