Flashing Linux on i.MX7D

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flashing Linux on i.MX7D

1,585 Views
kamilpacak
Contributor I

Hi, I want to flash any Linux on my i.MX7D board. It is possible? 

Tags (3)
0 Kudos
1 Reply

816 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Kamil,

we have different BSPs for iMX7D with different kernel versions starting from 3.14.52 to 4.9. You can find them at Freescale Public GIT > fsl-arm-yocto-bsp.git - i.MX Linux BSP Release Yocto Project manifests 

There are also BSPs developed by a community external to NXP

Freescale · GitHub 

These BSPs are developed with Yocto. Below you can find a Yocto training for getting familiar with the process of building an image

Yocto Training - HOME 


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos