HI ,
In my project I have used IMX6Solo/Dual Lite Processor , We are gonna use live video streaming from processor to PC or laptop or cloud with resolution of 1080p@30fps . We are streaming the video via ethernet interface (1Gbps) . I refereed the errata sheets its clearly mentioned like , We can't able to achieve more than 400Mbps .
In our custom board , at 200Mbps itself not stable and facing error of 0.028% and I have tested with wandboard also . Same issue exist . I want to know how to overcome this issue , I need stabilize speed range for ethernet .
Kernel : Linux kernel 3.14.28
Processor : IMX6Solo/Duallite.
Note : Please find the iperf test of wandboard .
Hi ganesh
please check suggestions on
i.MX6 Gigabit Ethernet - Boundary Devices
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------