IMX6QP - SPI and DMA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6QP - SPI and DMA

1,510 Views
marcingrzelak
Contributor I

Hello,

How i should configure device tree to use ECSPI and DMA on IMX6QP (linux 4.1.15)? Do you hava any example?

Thanks!

Labels (2)
0 Kudos
1 Reply

739 Views
igorpadykov
NXP Employee
NXP Employee

Hi marcingrzelak

please look at linux/Documentation/devicetree/bindings/spi/fsl-imx-cspi.txt  

Since sdma/ecspi modules are the same as in i.MX6DQ/SDL one can look at example in

linux/arch/arm/boot/dts/imx6qdl.dtsi
http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/arch/arm/boot/dts/imx6qdl.dtsi?h=imx_4....

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos