AnsweredAssumed Answered

Cannot change Debian in my i.MX6ULL evk anymore

Question asked by Pablo Cottens on Oct 25, 2017
Latest reply on Oct 26, 2017 by CarlosCasillas

Hello, As stated above I have a i;MX6ULL evk board and I can't change the OS running in it anymore.

 

Initially I was using this tutorial on how to put debian 8 jessie on the board using mfgtool and everything worked accordingly. After a couple of months that I did this, I disconnected everything and reconnected everything in different ports and I am unable to detect the board with mfgtool since then.

 

I plugged both micro-usbs to the computer and I can see that the serial usb used for viewing the logs is detected without a problem, but the other one doesn't seem to be recognized by windows anymore.

 

It takes a while, but after a few seconds of being connected to the PC D2003 starts blinking (the LED located between the power connector and the board with the processor) and whenever I disconnect it it stops blinking, but still, windows doesn't seem to detect it and mfgtool says that there is no device connected.

Outcomes