Enabling Power on Self Test (POST) IMx6solox

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enabling Power on Self Test (POST) IMx6solox

1,388 Views
niranjanbc
Contributor IV

Hi

I am looking to enable the "POST" (POST_CONFIG) in U-boot running on IMX6SoloX, to enable that i need non volatile memory address for _POST_WORD_ADDR. do we have any solution for that. can use the NOR flash address i have my board or it should be onchip memory only.

THANKS

Niranjan

Labels (3)
2 Replies

906 Views
igorpadykov
NXP Employee
NXP Employee

Hi Niranjan

I am afraid "POST" is not supported in nxp uboot releases and
this may be posted on uboot mail list
https://lists.denx.de/listinfo/u-boot

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

906 Views
niranjanbc
Contributor IV

Thanks for the response Igor,

we are looking for some thing like POST to do bare minimal test on power up.

if POST is not supported do we have any other option for self test.

For 1 Gbyte DDR ram test i see there is a mtest, but which is very slow. 

thanks

Niranjan

0 Kudos