IMX6Quad Standalone Bare-metal application

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6Quad Standalone Bare-metal application

467 Views
ailtonlopes
Contributor III

Hi,

 I'm designing one custom system on the i.mx6Quad . I want to use it for standalone bare-metal environment on it. Do you have any standalone peripheral test codes for i.mx6Quad processor? if yes please send me the source codes.  are you providing full fledged updated source code for all the peripherals?

 How to compile the i.mx6 bare metal source code? is there any IDE to compile the bare metal source code? if yes then is it freely available in the web ? if yes please send me the link.

 Is it possible to debug the standalone applications on IDE?

 Im looking forward for your valuable information.

Kind Regards

Ailton Lopes

Labels (1)
0 Kudos
1 Reply

293 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ailton

please look at baremetal sdk examples

Github SDK
https://github.com/backenklee/swp-report/tree/master/iMX6_Platform_SDK

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos