AnsweredAssumed Answered

How can I synchronize the ADC conversation with the PWM Output Block ?

Question asked by Leon Thürnau on Oct 23, 2017
Latest reply on Dec 20, 2017 by Leon Thürnau
Branched from an earlier discussion
Branched to a new discussion
How can I synchronize the ADC conversation with the PWM Output Block, so that the conversation definitly isn't started in the rising or falling edge ?

 

 

I want to Trigger the ADC conversation after the PWM Output has a rising edge.

My idea is to set the Output Trigger in the Three_Phase_Output block. But which one ?

 

I saw this tab in the Three_Phase_Output block:

Where can I find the signals PWM X VAL n ?

 

The selected Output pin I should configure in the ADC config block.

But here after SYNC0 and ADCA Alternate Trigger are selected only this list is displayed.

 

Outcomes