My low power mode is stop,and I shut down all module,but my current sonsumption is very high,3.5mA.I don't know where consumes the current.
When my code enter stop mode ,I want to use the FXOSC to supply the precise time.So I set the ME.STOP.B.FXOSCON=1.At that time ,my current consumption is 3.5mA.But when I set the ME.STOP.B.FXOSCON=0,the current consumption is 2.1mA. I sad to know where consumes the current.I need help.Thks.
stop mode setting is below:
ME.STOP.B.PDO=1;
ME.STOP.B.MVRON=0;
ME.STOP.B.DFLAON=1;
ME.STOP.B.CFLAON=1;
ME.STOP.B.FXOSCON=0;
ME.STOP.B.FMPLL0ON=0;
ME.STOP.B.FMPLL1ON=0;
ME.STOP.B.SYSCLK=0xF;
ME.STOP.B.FIRCON=0;
Hi Peter,
My temperature is 25℃。I don't know what about the HPVREG? How I can switch off it ?
Hello,
Looks like you are close to the official currents measured during validation.
What about your temperature during measurement? As you can see it has big influence on current.
Peter