AnsweredAssumed Answered

Has anyone implemented Bluetooth on a K22F platform?

Question asked by David Pfaltzgraff on Oct 18, 2017
Latest reply on Oct 25, 2017 by David Pfaltzgraff

I have an embedded system based on the K22F and FreeRTOS. I was wondering if anyone has been able to implement Bluetooth in a similar environment.The objective is to be able to use it in the SPP mode to eliminate the cable as well as be able to connect to USB devices that don't support the CDC protocol like smart pones, etc.

 

If so, what hardware was used for the Bluetooth?

 

Also, what libraries are available?

 

Thanks.

Outcomes