i.MX6 AUDMUX passthrough

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 AUDMUX passthrough

Jump to solution
580 Views
marinusleeuweri
Contributor I

Hello,

For an application I have to send signals coming from a microphone with an RF transceiver. For additional processing I want to connect I2S busses also to the i.MX6, for a reference on a solution that probably works see attached figure.

audmux_implementation.png 

Now I wonder, does the i.MX allow for passthrough, from external to external port, and which does not cost CPU time? This would make the schematic considerably easier, as shown in the Preferred solution.

Can anyone tell me if this is possible?

Kind regards,

Marinus 

Labels (1)
1 Solution
428 Views
igorpadykov
NXP Employee
NXP Employee

Hi Marinus

in general this is possible, please check AN2628 Programming Audio Applications

https://www.nxp.com/docs/en/application-note/AN2628.pdf 

Best regards
igor
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
429 Views
igorpadykov
NXP Employee
NXP Employee

Hi Marinus

in general this is possible, please check AN2628 Programming Audio Applications

https://www.nxp.com/docs/en/application-note/AN2628.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos