AnsweredAssumed Answered

FreeRTOS adapter for Freescale USB stack 5.0?

Question asked by SCOTT MILLER on Oct 18, 2017
Latest reply on Oct 26, 2017 by Daniel Chen

I'm still using the v5.0 beta of the Freescale BM USB stack and I'm curious if there's an RTOS adapter for it already written for FreeRTOS.  I realize it's deprecated but switching to KSDK and MCUXpresso is simply not an option right now - I've got deadlines to meet and that's going to be hard enough without switching tools in the middle of everything.  It's working well enough now but I see that it supports running as a task in MQX, and if I can do the same in FreeRTOS to reduce the amount of processing done in interrupt context, that would be useful.

 

Thanks,

 

Scott

Outcomes