AnsweredAssumed Answered

Questions about MPC5674F

Question asked by LEE on Oct 17, 2017
Latest reply on Oct 18, 2017 by David Tosenovjan

I have two questions about MPC5674F

 

1. Where can i find a __start function in a generated project ?

    I have not implemented the __start function in the generated project, but       the generated project seems to be run after _hardware_init is called by a          __start function that is not implemented in code.

   Can i see an defualt code information for the __start function ?

 

2. I recently implemented SRAM cache activation code with your help. 

    I also have made sure that the i-cache works normally by checking a i-            cache list through a debugger.

    However, the d-cache seems to not work normally. (a d-cache list was not      assigned anything)

    Do I need to implement an additional initialization code to use the d-                cache?

    Or, do I need to initialize the SRAM(or the stack) after initializing the d-            cache?

Outcomes