AnsweredAssumed Answered

关于VPU编码的问题

Question asked by juzi chen on Oct 17, 2017
Latest reply on Oct 22, 2017 by juzi chen

之前在IMX6DL3.0.35内核版本上,利用V4L2框架获取YUV422视频,通过IPU转码成YUV420,再通过VPU硬编码已经完成!

    现在我需要移植到L3.14.52内核上,需要做哪些改变?2个版本的VPU编码是否存在差异?

    应用程序不改变时,运行时的一些log

    imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_9 = 0x04000000

    mxc_mipi_csi2 21dc000.mipi_csi: mipi_csi2_reset: mipi_lane_bps = 324 Mbps

    mxc_mipi_csi2 21dc000.mipi_csi: mipi_csi2_reset: value = 0x48.

    imx-ipuv3 2800000.ipu: handler already installed on irq 20.Error registering rot irq

    VIDIOC_STREAMON error

    imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00100000

    imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_9 = 0x04000000

    imx-ipuv3 2400000.ipu: ERR:[0xa88e4000]-no:0xd0 "wait_for_comp_timeout" ret:0,line:2967

    imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_9 = 0x04000000

    imx-ipuv3 2400000.ipu: ERR:[0xa88e2e00]-no:0xe0 "wait_for_comp_timeout" ret:0,line:2967

    imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_9 = 0x04000000

    imx-ipuv3 2400000.ipu: ERR:[0xa88e2e00]-no:0xf0 "wait_for_comp_timeout" ret:0,line:2967

    imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_9 = 0x04000000

    imx-ipuv3 2400000.ipu: ERR:[0xa88e2e00]-no:0x100 "wait_for_comp_timeout" ret:0,line:2967

    imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_9 = 0x04000000

    imx-ipuv3 2400000.ipu: ERR:[0xa88e2e00]-no:0x110 "wait_for_comp_timeout" ret:0,line:2967

    imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_9 = 0x04000000

这些好像是IPU的问题,当我把IPU关掉不用然后,再从V4L2那边直接获取YUV420视频格式的码流,直接VPU编码,能够编码,但是没有SPS和PPS字符串,全部是I帧和P帧。这个是什么问题?

而当我手动的把3.0.35上编码获得的SPS和PPS写到3.14.52编码后的avi文件时,播放的情况是这样的:如附件所示:

SPS:0x00,0x00,0x00,0x01,0x67,0x42,0x40,0x1e,0xa6,0x80,0xb0,0x12,0x64

PPS: 0x00,0x00,0x00,0x01,0x68,0xce,0x30,0xa4,0x80

出现这种图像叠加的情况,这个又是怎么问题呢?

 

谢谢!

Attachments

Outcomes