MEMORY
{
/* FLASH: 0x00000000 - 0x0003FFFFF */
/* Fixed location required for RCHW and program entry point*/
resetvector: org = 0x00000000, len = 0x00000008
/* Contains initializations from __ppc_eabi_init.c,
MPC56xx_HWInit.c, MPC56xx_init_*.c and the entry point (__startup).
Should be 4K since the hardware automatically creates a default TLB entry
from the start of the entry point specified in RCHW.
*/
init: org = 0x00000010, len = 0x00000FF0 /* ~4K */
/* ~63K gap required to align the exception handlers.*/
/* Contains interrupt branch tables for both core and INTC module
and the ISR handlers code. Note, the gap is required since the vector
base address field of core IVPR is defined within the range [0:15], the
INTC branch tables must be loaded at an address aligned to 64K boundary.
*/
exception_handlers: org = 0x00010000, len = 0x0020000 /* 128K */
/* Space allocated for user code and device initialization.
ROM Image address should be set with the start address of this
segment in order to instruct the runtime to initialize the
static variables. All the section above are ignored for this action.
Please see -romaddr linker option.*/
internal_flash: org = 0x00030000, len = 0x003D0000 /* 3904K */
/* SRAM: 0x40000000 - 0x4003FFFF */
internal_ram: org = 0x40000000, len = 0x00030000 /* 192KB */
heap : org = 0x40030000, len = 0x00008000 /* 32KB Heap start location */
stack : org = 0x40038000, len = 0x00008000 /* 32KB Start location for Stack */
/* ROM SW ID */
rom_sw_id: org = 0x40035000, len = 0x0000000D
}
SECTIONS
{
GROUP : {
/* I want to fill the value of symbol */
} > rom_sw_id
}
Hi,
I would suggest you submit a private case for this question.
https://community.nxp.com/docs/DOC-329745
Please detail what result you expect.
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------