AnsweredAssumed Answered

LPC824 - IRC - quoted 12MHz +/- 1.5%

Question asked by Paul Sanders on Oct 13, 2017

Is there any avalible graphed data showing typical curves?

 

Vs Voltage

Vs Temp

Vs ageing

 

Also is the following qualified? i.e. what is the accuracy below 2.7V?

 

"Conditions: Frequency values are typical values. 12 MHz  1.5 % accuracy is guaranteed for
2.7 V  VDD  3.6 V. Variations between parts may cause the IRC to fall outside the 12 MHz 
1.5 % accuracy specification for voltages below 2.7 V."

Outcomes