I have ported Android Marshmallow 6.0.1 into imx6 sabresd Board and flash the image to Board. I'm facing camera problem , couldn't open the camera.
Please find the attachment of CTS failure list. Hope do you have any idea. Please consider my request to solve my problem.
Original Attachment has been moved to: host_log_4493427107813570818.zip
Original Attachment has been moved to: device_logcat_6619181058126652047.zip
Hi,
Thank you for responding mail.
Usually, I had followed that same reference documents only.
i.e android_M6.0.1_2.1.0_docs.tar.gz
can you help me , how to solve the problem ?
Thanks & Regards,
Lakshmikanth
Which camera are you using?
Hi,
Thank you for reply.
The Board contains inbuilt camera i.e ( MIPI camera) . Unable to open the camera.
Thanks & Regrads,
Lakshmikanth R
Hello,
Do you are using out BSP? This is because our BSP normally support the use of the cammer.
If not, try building the Android image with our BSP.
In the below link, you can find the Android documentation and BSP.
Android OS for i.MX Applications Processors|NXP
Best Regards,
Diego.