AnsweredAssumed Answered

P4080PCIE usdpaa_pcie error

Question asked by Song Lee on Oct 13, 2017

When I use P4080PCIE, I encounter the following problems:

[root@p4080 /root]# /etc/rc.d/init.d/usdpaa_pcie start
Creating fsl-usdpaa-pciemem file:
cpu5/5: ! CRITICAL FM-Port Error [drivers/net/dpa/NetCommSw/Peripherals/FM/Port/fm_port.c:3192 FM_PORT_Disable]: Invalid State;
cpu5/5:
cpu5/5:
cpu5/5: ! CRITICAL FM-Port Error [drivers/net/dpa/NetCommSw/Peripherals/FM/Port/fm_port.c:3192 FM_PORT_Disable]: Invalid State;
cpu5/5:
cpu5/5:
Starting USDPAA Packet Driver:
No network interfaces are available

 

[root@p4080 /root]#

 

Note:
P4080 10 Gigabit network card interface is connected to another x86 Gigabit Ethernet card network port.

Outcomes