AnsweredAssumed Answered

SPI data transfer using DMA and PIT?

Question asked by Santosh Alagawadi on Oct 13, 2017
Latest reply on Oct 19, 2017 by Santosh Alagawadi

SPI data transfer using DMA and PIT

 

uC: MPC 5643

 

1. Want to send 5 SPI commands for 20 times with PIT configuration.

2. Configure PIT0 for time x and PIT1 for 20 * x and send first 5 SPI commands in DMA and retrigger the same set of commands for 20 times.

3. Once 20 iterations completed, PIT1 must trigger interrupt and disable PIT

4. This I am trying to achieve without software intervention, the software intervenation will be after 20 iteration to service the interrupt.

5. I am not able to achieve this with MPC56, How can achieve this? Is there any dependency

6. The PIT0 is not triggering DMA after first transfer, configured the registers in DMA_MUX, Once the PIT0 triggers DMA data transfer, do we need software intervantion or it is possible to send data transfer without software intervation?

Outcomes