MPC5746R eTPU requirement for IGF

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5746R eTPU requirement for IGF

936 Views
jamesmurray
Contributor V

It seems that eTPU2 inputs require that the Input Glitch Filter (IGF) is configured before they will work.

Is this mentioned in the MPC5746RRM ? I don't seem able to find it. Only by chance did I stumble upon this critical information in the 5634M - 5746R migration guide document.

It would be handy to have a code snippet showing the multiple configurations required to get an eTPU pin to actually be an input.

e.g.

MPC5634M code was simple:

SIU.PCR[114].R = 0x0503; /* Configure pad for primary eTPU_A[0] input and PU */

MPC5746R appears to require lots more if I'm understanding it correctly:

    SIUL2.MSCR0_255[39].R = 0x003d0000; /* Configure PC7 pad for primary eTPU_A[0] input and PU */
    SIUL2.MSCR512_995[576-512].R = 1; /* set as eTPU_A TCRCLK_A input */
    SIUL2.MSCR512_995[652-512].R = 1; /* PC7 -> IGF0 -> eTPU_A0 */

    /* Configure input glitch filter for crank and cam inputs as bypass */
    IGF.MCR.B.MDIS = 0;
    IGF.MCR.B.FGEN = 0;
    IGF.MCR.R = 0; /* set rising and falling to bypass */
    IGF.MCR.B.FGEN = 1; /* enable filter */

James

0 Kudos
6 Replies

621 Views
jamesmurray
Contributor V

How about when using it as a TRCLK input?

I will retest my code later in the week, but until I added the IGF configuration, nothing seemed to be happening.

James

0 Kudos

621 Views
jamesmurray
Contributor V

Well.... I tested this with my IGF setup code removed and it still works ?!

So, looks like I raised a false alarm. Sorry about that. I'm not sure why I couldn't get it working initially though.

However, please explain what this means in AN4658

"After system reset, the IGF modules are in Configuration mode by default. This mode disables IGF output and prevents the signals from the pins from reaching the eMIOS and eTPU modules"

James

0 Kudos

621 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I was also testing it with MPC5777C device where really it is needed to configure IGF module, but MPC5777C used different pads, it works slightly different way:

Example MPC5777C-eTPU_GPIO_test GHS714 

Back to MPC5746R:

Author of AN4658 no longer works in the company so I cannot check it with him. It is possible some preliminary version had it implemented this way. Also Figure 45-1 in RM seems to me unclear. I will ask for changing it to see direct path between pad and IOMUX.

621 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

As I know Input Glitch Filter is new option available on MPC57xx devices, it is not part of eTPU2 (already use with some MPC56xx). It is not necessary to use it, you may use backward compatible option and route these signal directly to eTPU module.

pastedImage_1.png

pastedImage_2.png

0 Kudos

621 Views
jamesmurray
Contributor V

In my testing that did not work.

AN4658 says "After system reset, the IGF modules are in Configuration mode by default. This mode disables IGF output and prevents the signals from the pins from reaching the eMIOS and eTPU modules"

MPC5746RRM doesn't appear to mention this.

James

0 Kudos

621 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I have just tested it and it works on my side as expected. Having connected eTPUB0 (general purpose output) and eTBUB1 (general purpose input) together, I am able to read inputs values without setting of Input Glitch Filter properly.

pastedImage_2.png

0 Kudos