AnsweredAssumed Answered

Managing BAF in MPC5777M

Question asked by Paulo DA SILVA PINTO on Oct 11, 2017
Latest reply on Oct 12, 2017 by Peter Vlna


With DO178 level A, we need to master all executed code in the platform.

1°) Is it possible to have the source code of the BAF ?

2°) if not, is it possible to overrun the BAF code and run our code defined at our own reset address. Maybe, there is a way to change the SSCM_PSA register ?

3°) Peter Vlna has answered in MPC5777M BAF  that it is possible to erase the BAF sector. If I would like to put our customer boot, how can I do that ?


Thank you