eth0 and can0 not working simultaneously on imx6q-sabreboard AI(automotive infontainment)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eth0 and can0 not working simultaneously on imx6q-sabreboard AI(automotive infontainment)

337 Views
sandeepkumar12
Contributor I

hi ,

i am working on imx6q-sabre AI board .but when enables the CAN0  up only the CAN works, if enables the ethernet at the same time it s not works,(due to pin conflicts with flexcan1).

i checked the imx6q-sabreauto-flexcan1.dts file is only enables the flexcan1 and disables the fec(fast ethernet controller).

is, there any way i can use simulataneously both ethernet and CAN communication.

            OR is there any boards available for overcome this issue.

please reply soon anyone .

thanks 

sandeep kumar

0 Kudos
0 Replies