AnsweredAssumed Answered

DRAM Initialization problem in u-boot on android  Prebuilt-Image for SCM i.MX6Q 1GB QWKS REVC  board

Question asked by Manoj Sampathkumar on Oct 5, 2017
Latest reply on Oct 10, 2017 by Manoj Sampathkumar

Hi,

 

I am using SCM i.MX6Q 1GB QWKS REVC board . I tried to boot the board with the Prebuilt-images of android. (images_M6.0.1_2.1.0-ga_MX6SCM).

 

I partitioned the sd card using fsl-sdcard-partition.sh and placed the images in sd card as instructed in the manual.

But when i tried to boot the board i am facing DRAM Initialization problem in uboot level

 

U-Boot 2015.04-00008-gcac6ef2 (May 05 2017 - 17:00:08)

CPU: Freescale i.MX6Q rev1.5 at 792 MHz
CPU: Temperature 37 C
Reset cause: POR
Board: MX6DQSCM-QWKS-REV3
I2C: ready
DRAM:

 

After this the board hangs. Is there any lastest prebuilt images or how to fix this issue.

 

Thanks,

Manoj

Outcomes