Here is the error message:
GStreamer-CRITICAL **: gst_element_link_pads_filtered: assertion 'GST_IS_BIN (parent)' failed
The command:
gst-launch-1.0 imxv4l2videosrc device=/dev/video0 num-buffers=100\
! video/x-raw,format=\(string\)GREY8,width=2592,height=1944,framerate=\(fraction\)15/1 \
! queue \
! imxvpuenc_h264 \
! $ qtmux \
! filesink location=file.mov
I am running yocto linux on i.mx6 quad sabresd and I an trying to get the input from the camera.
Any suggestions?
Hi Lorenc
please try nxp bsps described on
and follow Linux Guide from doc package (link below) for using gstreamer
Note there are two kinds of gstreamer described on
trac.gateworks.com/wiki/Yocto/gstreamer
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Which BSP should I try. There seem to be many.
please try latest Linux 4.9.11_1.0.0
~igor