Hello all,
I tried to setup most of the MCG modes with PE to present this within a lecture. While doing this I discovered a behavior related to the external RTC and slow internal clock that is unclear to me and maybe someone can explain it.
Interestingly the slow internal clock on the K60FN1M is running also on 32kHz like the external RTC clock. So that might be a hint about the source of the problem or about how to avoid or workaround it.
Anyone successfully running a K60FN1M from the external RTC or from the slow internal clock?
Best Regards
Markus
Hi Markus,
Sorry for the late reply!
Please refer the attached RTC_LDD example. I have test it on TWR-K60F120M board with CodeWarrior10.7.
Best Regards,
Robin
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------