when i connect board using minicom it is booted from the emmc and when i try to modify the wpa_supplicant.conf it says that permission denied even though i work as root usiung 'su' and its also stated that read only file system i even tried to remount it but it says your directory is not in /proc/mnt
imx6ulevk imx6ultralite #imx6ulnxpuiopb #i.mx6 android #androidthings #wpa_supplicant #simple interrupt gpio #gpio-leds
Hi yash
please refer to sect.4.12 Wi-FI BCM4339 attached Linux Manual
for supported wifi modules in nxp official bsps described on
If other module is used, support may be provided by vendor of used module.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------