AnsweredAssumed Answered

Can I set up the step-by-step CPU FREQ. control at high alarm (using thermal driver).

Question asked by Cheolhyeon Cho on Sep 28, 2017
Latest reply on Sep 28, 2017 by igorpadykov

Dear Mr./Ms.

I know i.mx6 has the thermal driver for preventing damage from over-heating of cpu.

In driver code, the alarm levels are 85 degree, 105 degre, It is only 2 step levels.

 

When the cpu temp. is reached to passive level (85), the cpu freq is set-up into the lowest freq. by the thermal driver right now.

There are four frequencies in the cpu freq table of i.mx6 1GHz version, so if the passive level is reached, it would be more efficient to adjust the cpu freq. step by step. Is there the method for a step-by-step adjustment?

 

Cheol-Hyeon Cho,##

Outcomes