Hello all,   I am working with a mcf5484Lite evalutaion b...

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hello all,   I am working with a mcf5484Lite evalutaion b...

882 Views
raulen
Contributor III
Hello all,
 
I am working with a mcf5484Lite evalutaion board. I downloaded the last revision of ltib for this processor (mcf547x/8x). If I just configure LTIB with prebuilt options, it works perfectly, but If I try to add some packages like gdbserver or expat, the LTIB tries to connect somewhere, but it fails.
My internet connection is located after a proxy. So I guess this is the problem. How should I configure the .ltibrc in order to get it works?
 
Thanks in advance,
Raúl
Labels (1)
0 Kudos
1 Reply

196 Views
fsl_linux_spt
Contributor III
You need to set the proxy settings in the %http_proxy section.
Then you need to set the %gpp_proxy to 1.
0 Kudos