Trouble debugging my project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Trouble debugging my project

1,032 Views
emilbackram
Contributor I

Hi

I'm having truble debugging my project when I try to "step into (F5)" or "step over (F6)" the PLL configuration, but if I set a breakepoint after the PLL configuration and click " resume (F8)" it works well. Am I doing somthing wrong or is it a bug in the debugger?

(I'm using the S32 DS and the MPC5746R processor.)

Thanks //Emil

0 Kudos
2 Replies

968 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

what is the state of PLL when changing the configuration?

pastedImage_1.png

Regards,

Lukas

0 Kudos

968 Views
emilbackram
Contributor I

Hi Lukas

I am only configuring the PLL at startup ( as you can see in the attached immages), and I set the PLL0ON bit according to chapter 22.5.1.4 PLL initialization information in the reference manual.

Best regards

Emil

Från: lukaszadrapa

Skickat: den 6 oktober 2017 12:15

Till: Emil Backram <emil@freevalve.com>

Ämne: Re: - Re: Trouble debugging my project

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: Trouble debugging my project

reply from Lukas Zadrapa<https://community.nxp.com/people/lukaszadrapa?et=watches.email.thread> in Other NXP Solutions - View the full discussion<https://community.nxp.com/message/949752?commentID=949752&et=watches.email.thread#comment-949752>

0 Kudos