I.MX6UL的MQS功能要驱动大功率喇叭,用哪种功放IC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6UL的MQS功能要驱动大功率喇叭,用哪种功放IC

2,247 Views
jinshengzhao
Contributor I

你好,I.MX6UL的 RM 中提到的音频功能MQS,

MQS is used to generate medium quality audio via a standard GPIO in the pinmux. The
user can connect stereo speakers or headphones to a power amplifier without an additional DAC chip.

但是网上的MQS的资料非常少。那么

1、MQS的输出波形是什么样式的?是不是类似SPWM?

2、MQS的输出功率是怎么样的?从上述英文来看只能接32Ω的耳机

3、MQS如果要外接大功率的喇叭,用哪种类型的功放芯片?A类?B类?D类都可以吗?

4、与功放的电路怎么接呢?是不是和普通的DAC输出的音频接法一样?

Labels (1)
Tags (1)
0 Kudos
2 Replies

1,354 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello jinsheng,

    MQS是输出的PWM音频波,RIGHT和LEFT引脚直接接耳机,可以驱动并听到声音。如果需要放大的话,2个引脚各接一个NPN型三极管(接在B极,C极输出)就可以实现放大功能。

    所以,你如果需要接放大器,你只需要把它们作为不带编码的数字信号,进行放大就可以了。接哪个类型的放大器,没有特别要求。


Have a great day,
TIC  Weidong Sun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,354 Views
jinshengzhao
Contributor I

是不是像下面的驱动电路即可?

MQS的驱动图片.png

0 Kudos