AN5327(3-phase Sensorless Single-Shunt Current) question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AN5327(3-phase Sensorless Single-Shunt Current) question

948 Views
bjhwang
Contributor I

Dear Sir or Madam,

I have a question related to this AN5327SW.

Currently, this SW runs the motor by using MCAT tool.

Is there some advice or other example that runs with LIN communication?

Thanks

Best regards

0 Kudos
2 Replies

583 Views
bjhwang
Contributor I

Dear Sir,

Thank you for the reply. From your advice I tried to combine the application note AN5327 / AN5122.

Not like application notes, I set the MCU slave S12ZVML128 and made cfg file. After that I put all the LIN Driver from the AN5122 to AN5327 and made access path to it also. Lastly, I include "Lin.h" and build the project. The compile progress was ok, but when I debug this application notes, this failed to resume target process. downloading binary to target... messages comes out. 

Could you tell me this?

Thanks

0 Kudos

583 Views
pachamatej
NXP Employee
NXP Employee

Dear BJ Hwang,

As far as I know, there is no example available combining LIN communication and motor control application for S12ZVML.

But you can combine two application notes AN5327 and AN5122 available at S12ZVM Mixed-Signal MCUs|MagniV|NXP 

Since the AN5327 is controlled by FreeMASTER - MCAT interface, the only change would be necessary only if the SCI hardware pins overlap the LIN communication pins. Then you would have a possibility to debug the communication using FreeMASTER as well.

Best regards,

Matej

0 Kudos