SPC5777C VDDE2 and VDDE2A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPC5777C VDDE2 and VDDE2A

Jump to solution
670 Views
liuxingqiao
Contributor I

Hello,

   Could anyone tell me what is the relationship between VDDE2 and VDDE2A supply pins of SPC5777C? Could they be tied to different voltages, for example, VDDE2 tied to 5V and VDDE2A tied to 3.3V?

   Thanks in advance.

   Best regares,

   Liu xingqiao

0 Kudos
1 Solution
563 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

There is none. In the device predecessor (MPC5676R) it was one domain. On the MPC5777C it has been split onto 2 domains (in order to minimize I/O pins affected when using Ethernet).

Yes, they can be tied to different voltages, as you shown in the example.

View solution in original post

1 Reply
564 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

There is none. In the device predecessor (MPC5676R) it was one domain. On the MPC5777C it has been split onto 2 domains (in order to minimize I/O pins affected when using Ethernet).

Yes, they can be tied to different voltages, as you shown in the example.