AnsweredAssumed Answered

The problem about shutdown or reboot on IMX6(DL/Q) with Android6.0.1

Question asked by peng xingwei on Sep 22, 2017

Hi all,

      I come cross a problem about shutdown or reboot, my board can't shutdown and reboot by using power button

the log as follows when I type the  reboot  command and the system is halt

   

root@sabresd_6dq:/ # reboot
sysrq: SysRq : Emergency Remount R/O
EXT4-fs (mmcblk3p6): re-mounted. Opts: (null)
EXT4-fs (mmcblk3p4): re-mounted. Opts: (null)
Emergency Remount complete
imx2-wdt 20c0000.wdog: Device shutdown: Expect reboot!
reboot: Restarting system with command ''
Reboot failed -- System halted

 

 

and when I enter the power button to power off ,as follow  ,the system is halting

 

 

About the problem above,How to solve it ?? Thanks

Outcomes