S32v234 - EVB compatibility with swapping to S32 DS for Vision 2.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32v234 - EVB compatibility with swapping to S32 DS for Vision 2.0

1,342 Views
loganphillips
Contributor I

I have recently updated to the new S32 DS 2.0, and I followed the tutorials. When I have tried to run the application on the S32 EVB, it will not completely run, and I get Segmentation faults. When I run similar 'demos' using S32 DS v1, it works fine. Is there anything I need to do to swap over to the new S32 DS 2.0?

It seems to be exiting in the sdi_io.cpp 

The tutorial I follow is the isp demo using the mipi simple graph.

Side note, there are some inconsistencies in the video and pdf. I've tried all the ways.

Any information will be helpful.

0 Kudos
5 Replies

990 Views
jiri_kral
NXP Employee
NXP Employee

Hello, 

Did you properly allocated DDR buffers ?  In attachment is mipi_simple graph and mipi_simple_app projects which are working in S32DS v2.0. 

Jiri 

0 Kudos

990 Views
loganphillips
Contributor I

I just tried this version, and it did not work either. When I create a project from example in S32DS v1.0 using the isp_csi_dcu_linux example, it works fine. 

I received the EVB and an SD card back in early 2016, would there be changes causing the problem?

0 Kudos

990 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

this is strange. I have older board too - and it is working normally. 

My linux version on the EVB is (uname -a): 
Linux s32v234evb 4.1.26-rt29 #1 SMP PREEMPT Wed Apr 12 20:47:45 CEST 2017 aarch64 GNU/Linux

and I tried this example with EVB version 700-28899 REV X13 and 700-28899 REV A. Example is working normally. In attachment is elf file for linux running on EVB. 

Jiri

0 Kudos

990 Views
loganphillips
Contributor I

Linux version: Linux treerunner 4.1.26-rt29 #1 SMP PREEMPT Mon Nov 14 20:44:55 CET 2016 aarch64 GNU/Linux

EVB: SCH-28899 REV D   -   700-28899 REV X13

The file faulted out in a similar way.

EDIT: I noticed that the "S32V234.h" file in the working application is on REV 1.2.0A and the file you sent me was REV 2.1

0 Kudos

990 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

you have the very same HW and linux version. May be you have some HW issue with your EVB?. Anyway - I can't reproduce the seg. fault state on my EVB.

Jiri 

0 Kudos