AnsweredAssumed Answered

OM26630FDK Questions

Question asked by Dong Hyeon Lim on Sep 20, 2017
Latest reply on May 8, 2018 by Muralidhar M

There is one question.

 

I have the OM26630FDK (CLEV6630B board, CLRC663 PLUS).
If there is a UART port in this FDK, I want to transfer data to another module via UART communication. (The module I'm talking about here is a demo board for Bluetooth development.)


However, I am not sure what part of the FDK should be utilized.

When I think of it, I think it is possible through the part shown in the picture below.

 

 

According to my study, it is judged that the indicated part is TXD0 and RXD0 of LPC1769, so I think this part can be used for UART communication.

 

Here are my questions: Does the OM26630FDK have a UART port? If so, can I use it to transfer data to another module?

Outcomes