Hi,
I'd like to know the tolerance of ENVADJ voltage. Also, what is voltage source of ENVADJ?
The ENVADJ field adjusts the trip point for the envelope detector.
000 = Trip-Level Voltage is 0.12500 V
001 = Trip-Level Voltage is 0.10000 V
010 = Trip-Level Voltage is 0.13750 V
011 = Trip-Level Voltage is 0.15000 V
1XX = Reserved
Best Regards,
Sugiyama
Hello Toshishisa,
The voltage setting is used to set the trip point for the envelope detector, and evelope detector will determine if the current usb signal on differential line is valid according to the voltage.
Have a great day,
TIC weidong sun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi, weidong sun,
Thank you for the answer.
However, I'd like to know below items of ENVADJ voltage.
1. How this voltage generate in circuit? From USB LDO?
2. How much the voltage vary by each device? When 000=125mV, does the voltage vary +/-5mV?
3. How much the voltage vary depend on temperature? About 35degC, the voltage seems minimum.
Best Regards,
Sugiyama
Hi,
Could you answer?
Best Regards,
Sugiyama