I am using a Silex SDCAN2 module with MCIMX6ULL EVK. The SDCAN2 module works well in Wi-Fi Client mode however fails to work in AP mode. Hostapd is used for enabling AP mode. The AP mode comes up for a short interval and then dies out with no failure prints coming up on hostapd. The interface is also up and available on the host.
Hi Prashant
silex modules are not supported in nxp official bsps starting from L3.14.52.
One can try to port older releases found on
or apply to silex support (Contact Silex Support ) for updated driver or look at third party releases
New Silex WiFi 802.11ac and BT4.1 module - Boundary Devices
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------