Hi,
Trying to develop a simple CAN driver code with the functionality to transmit and receive the CAN packets.
CAN4 channel is being used and RCW settings are loaded to enable CAN4_tx and CAN4_rx.
Attached is the code used for reference.
On transmitting the simple CAN packet, we are getting the stuff error as shown in the attached snapshot.
Also please find the CAN transceiver schematic used.
Kindly support us in resolving this issue. Please let me know if you need more information.
Original Attachment has been moved to: 1000BASET1_TWR_RAM-core0_Rev0.1.zip
Test your board if MCR[SRXDIS] bit is cleared and Loopback mode is enabled.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------