AnsweredAssumed Answered

Incorrect values are shown in the peripherals+ view

Question asked by Eric Qin Employee on Sep 20, 2017
Latest reply on Sep 27, 2017 by Alice_Yang

Incorrect values are shown in the peripherals+ view when I debug “flexcan interrupt transfer ”of SDK2.2.0 and view the value of CAN0-CTRL1 register with TWRKV46F150M and MCUXPresso v10.0.2 [Build 411]. As shown below, the bit fields named BOFFREC, RWRNMSK, LPB, CLKSRC and ERRMSK only have one bit, but why is the value bigger than 1  shown in the bit fields? What are meaning of “Value_0” or “Value_1”shown in some bit fields?

Outcomes