Touch input and focus issue in android kitkat

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Touch input and focus issue in android kitkat

514 Views
archanaharish
Contributor I

Hi ,

We are porting android kitkat to SAMA5D3 development board which is of size 480*272  (pixel), only partial touch input is happening like drop down and Setting page when I keep giving inputs randomly and nothing else. But touch works well with  Evaluation Kit which is of size 800*600 (pixel length).

 

The cause of touch issue is, it is taking requested height as 19 instead of 480 in WindowManagerService. Please refer the below log.

 

I/WindowManagerService( 1418): relayoutWindow  win.mRequestedWidth272
I/WindowManagerService( 1418): relayoutWindow  win.mRequestedHeight19
I/WindowManagerService( 1418): AOSP:::updateFocusedWindowLocked
I/WindowManagerService( 1418): AOSP:::computeFocusedWindowLocked

Any help will be appreciated.

Original Attachment has been moved to: logs.zip

Labels (4)
0 Kudos
1 Reply

410 Views
igorpadykov
NXP Employee
NXP Employee

Hi archana

one can try Calibrate.APK as described for example on

How-To: Fix Touchscreen Issues in Android Phones 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos