AnsweredAssumed Answered

LS1021A  : When I bitbake fsl-image-full in the ubuntu14.04,errors occurs.

Question asked by 黄 皓 on Sep 20, 2017
Latest reply on Oct 4, 2017 by 黄 皓

the errors like this:

WARNING: Could not copy license file /home/huanghao/QorIQ-SDK-V2.0-20160527-yocto/build_ls1021atwr/tmp/work/ls1021atwr-fsl-linux-gnueabi/linux-qoriq/4.1-r0/git/COPYING to /home/huanghao/QorIQ-SDK-V2.0-20160527-yocto/build_ls1021atwr/tmp/work/ls1021atwr-fsl-linux-gnueabi/linux-qoriq/4.1-r0/license-destdir/linux-qoriq/COPYING: [Errno 40] Too many levels of symbolic links: '/home/huanghao/QorIQ-SDK-V2.0-20160527-yocto/build_ls1021atwr/tmp/work/ls1021atwr-fsl-linux-gnueabi/linux-qoriq/4.1-r0/git/COPYING'
ERROR: Function failed: do_configure (log file is located at /home/huanghao/QorIQ-SDK-V2.0-20160527-yocto/build_ls1021atwr/tmp/work/ls1021atwr-fsl-linux-gnueabi/linux-qoriq/4.1-r0/temp/log.do_configure.6316)
ERROR: Logfile of failure stored in: /home/huanghao/QorIQ-SDK-V2.0-20160527-yocto/build_ls1021atwr/tmp/work/ls1021atwr-fsl-linux-gnueabi/linux-qoriq/4.1-r0/temp/log.do_configure.6316
Log data follows:
| DEBUG: Executing python function sysroot_cleansstate
| DEBUG: Python function sysroot_cleansstate finished
| DEBUG: Executing shell function do_configure
| cp: cannot stat '/home/huanghao/QorIQ-SDK-V2.0-20160527-yocto/build_ls1021atwr/tmp/work/ls1021atwr-fsl-linux-gnueabi/linux-qoriq/4.1-r0/git/arch/arm/configs/ls1021a_defconfig': Too many levels of symbolic links
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_configure (log file is located at /home/huanghao/QorIQ-SDK-V2.0-20160527-yocto/build_ls1021atwr/tmp/work/ls1021atwr-fsl-linux-gnueabi/linux-qoriq/4.1-r0/temp/log.do_configure.6316)
ERROR: Task 47 (/home/huanghao/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-kernel/linux/linux-qoriq_4.1.bb, do_configure) failed with exit code '1'
NOTE: Tasks Summary: Attempted 2607 tasks of which 151 didn't need to be rerun and 1 failed.
Waiting for 0 running tasks to finish:

Summary: 1 task failed:
/home/huanghao/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-kernel/linux/linux-qoriq_4.1.bb, do_configure

I have no idea about this.Can anyone help me?

Outcomes