AnsweredAssumed Answered

Model Based Design Toolbox (MBDT) for MPC5643L controller

Question asked by Raghu Rajappa on Sep 19, 2017
Latest reply on Sep 19, 2017 by dumitru-daniel.popa

Hi,
I can see that there is MBDT and Motor Control Toolbox (MCT) for MPC5744P controller. There is also MCT for MPC5643L. But I cannot find MBDT for MPC5643L. Can I use the MCT blocks to continue model based design for the MPC5643L without any known issues? My intention is to generate code, program it onto the MPC5643L board and run SIL (Simulation in Loop), PIL (Processor in Loop) through Simulink to test functionality.

I ask this question because 5744P has two separate toolboxes while only one is available for 5643L. Is there a reason for this? 

Outcomes