AnsweredAssumed Answered

LPI2C RX FIFO PROBLEM

Question asked by Ravi Ranjan Kumar on Sep 18, 2017
Latest reply on Sep 19, 2017 by Ravi Ranjan Kumar

Hi,

      I am working on S32K144 LPI2C driver. While reading from slave(EEPROM), at a time I am able to read only 4 Bytes. If I am trying to read more than four bytes then garbage characters are coming except those four byte. After reading first four bytes, for next four bytes FEF bit is setting. I am trying to clear FEF by writing 1 but it is not clearing. 

                        How to transmit and receive data without using FIFO. if possible help with example code. I tried with S32K example code it is also with FIFO and I am facing same issue here also.

 

Please help.... 

 

Thanks and Regard,

Ravi Ranjan Kumar.

Outcomes