2GB Memory /16GB eMMC issue on iMX6 SoloLite

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2GB Memory /16GB eMMC issue on iMX6 SoloLite

531 Views
Sun1z
Contributor III

Hi All,

We're using i.MX6 sololite EVK (android N7.1.1_1.0.0-ga) as our development platform, now we want to make our board and change the 1GB LPDDR2 to 2GB LPDDR2 (or DDR3) as well as the eMMC from 8GB to 16GB. my question is that is it possible for us to use the mfg tool on the new board, if not, is there any source/patch available for that? thanks.

B.R.

Sun

Labels (3)
0 Kudos
1 Reply

405 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sun

please find new calibration coefficients for new board running ddr test

i.MX6/7 DDR Stress Test Tool V2.70 

put them to uboot/board/freescale/mx6slevk/imximage.cfg

and rebuild image. To use mfg tool on the new board

rebuild its firmware (files in firmware folder) using sect.6.2 Manufacturing

Tool, MFGTool attached Yocto Guide.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos