I can't understand the mean of below code,Is there some introduce document :
/* Entry Point */
ENTRY(Reset_Handler)
HEAP_SIZE = DEFINED(__heap_size__) ? __heap_size__ : 0x00000400;
STACK_SIZE = DEFINED(__stack_size__) ? __stack_size__ : 0x00000400;
/* If symbol __flash_vector_table__=1 is defined at link time
* the interrupt vector will not be copied to RAM.
* Warning: Using the interrupt vector from Flash will not allow
* INT_SYS_InstallHandler because the section is Read Only.
*/
M_VECTOR_RAM_SIZE = DEFINED(__flash_vector_table__) ? 0x0 : 0x0400;
/* Specify the memory areas */
MEMORY
{
/* Flash */
m_interrupts (RX) : ORIGIN = 0x00000000, LENGTH = 0x00000400
m_flash_config (RX) : ORIGIN = 0x00000400, LENGTH = 0x00000010
m_text (RX) : ORIGIN = 0x00000410, LENGTH = 0x0007FBF0
/* SRAM_L */
m_data (RW) : ORIGIN = 0x1FFF8000, LENGTH = 0x00008000
/* SRAM_U */
m_data_2 (RW) : ORIGIN = 0x20000000, LENGTH = 0x00007000
}
/* Define output sections */
SECTIONS
{
/* The startup code goes first into internal flash */
.interrupts :
{
__VECTOR_TABLE = .;
. = ALIGN(4);
KEEP(*(.isr_vector)) /* Startup code */
. = ALIGN(4);
} > m_interrupts
.flash_config :
{
. = ALIGN(4);
KEEP(*(.FlashConfig)) /* Flash Configuration Field (FCF) */
. = ALIGN(4);
} > m_flash_config
/* The program code and other data goes into internal flash */
.text :
{
. = ALIGN(4);
*(.text) /* .text sections (code) */
*(.text*) /* .text* sections (code) */
*(.rodata) /* .rodata sections (constants, strings, etc.) */
*(.rodata*) /* .rodata* sections (constants, strings, etc.) */
*(.glue_7) /* glue arm to thumb code */
*(.glue_7t) /* glue thumb to arm code */
*(.eh_frame)
KEEP (*(.init))
KEEP (*(.fini))
. = ALIGN(4);
} > m_text
.ARM.extab :
{
*(.ARM.extab* .gnu.linkonce.armextab.*)
} > m_text
.ARM :
{
__exidx_start = .;
*(.ARM.exidx*)
__exidx_end = .;
} > m_text
.ctors :
{
__CTOR_LIST__ = .;
/* gcc uses crtbegin.o to find the start of
the constructors, so we make sure it is
first. Because this is a wildcard, it
doesn't matter if the user does not
actually link against crtbegin.o; the
linker won't look for a file to match a
wildcard. The wildcard also means that it
doesn't matter which directory crtbegin.o
is in. */
KEEP (*crtbegin.o(.ctors))
KEEP (*crtbegin?.o(.ctors))
/* We don't want to include the .ctor section from
from the crtend.o file until after the sorted ctors.
The .ctor section from the crtend file contains the
end of ctors marker and it must be last */
KEEP (*(EXCLUDE_FILE(*crtend?.o *crtend.o) .ctors))
KEEP (*(SORT(.ctors.*)))
KEEP (*(.ctors))
__CTOR_END__ = .;
} > m_text
.dtors :
{
__DTOR_LIST__ = .;
KEEP (*crtbegin.o(.dtors))
KEEP (*crtbegin?.o(.dtors))
KEEP (*(EXCLUDE_FILE(*crtend?.o *crtend.o) .dtors))
KEEP (*(SORT(.dtors.*)))
KEEP (*(.dtors))
__DTOR_END__ = .;
} > m_text
.preinit_array :
{
PROVIDE_HIDDEN (__preinit_array_start = .);
KEEP (*(.preinit_array*))
PROVIDE_HIDDEN (__preinit_array_end = .);
} > m_text
.init_array :
{
PROVIDE_HIDDEN (__init_array_start = .);
KEEP (*(SORT(.init_array.*)))
KEEP (*(.init_array*))
PROVIDE_HIDDEN (__init_array_end = .);
} > m_text
.fini_array :
{
PROVIDE_HIDDEN (__fini_array_start = .);
KEEP (*(SORT(.fini_array.*)))
KEEP (*(.fini_array*))
PROVIDE_HIDDEN (__fini_array_end = .);
} > m_text
__etext = .; /* Define a global symbol at end of code. */
__DATA_ROM = .; /* Symbol is used by startup for data initialization. */
.interrupts_ram :
{
. = ALIGN(4);
__VECTOR_RAM__ = .;
__interrupts_ram_start__ = .; /* Create a global symbol at data start. */
*(.m_interrupts_ram) /* This is a user defined section. */
. += M_VECTOR_RAM_SIZE;
. = ALIGN(4);
__interrupts_ram_end__ = .; /* Define a global symbol at data end. */
} > m_data
__VECTOR_RAM = DEFINED(__flash_vector_table__) ? ORIGIN(m_interrupts) : __VECTOR_RAM__ ;
__RAM_VECTOR_TABLE_SIZE = DEFINED(__flash_vector_table__) ? 0x0 : (__interrupts_ram_end__ - __interrupts_ram_start__) ;
.data : AT(__DATA_ROM)
{
. = ALIGN(4);
__DATA_RAM = .;
__data_start__ = .; /* Create a global symbol at data start. */
*(.data) /* .data sections */
*(.data*) /* .data* sections */
KEEP(*(.jcr*))
. = ALIGN(4);
__data_end__ = .; /* Define a global symbol at data end. */
} > m_data
__DATA_END = __DATA_ROM + (__data_end__ - __data_start__);
__CODE_ROM = __DATA_END; /* Symbol is used by code initialization. */
.code : AT(__CODE_ROM)
{
. = ALIGN(4);
__CODE_RAM = .;
__code_start__ = .; /* Create a global symbol at code start. */
*(.code_ram) /* Custom section for storing code in RAM */
. = ALIGN(4);
__code_end__ = .; /* Define a global symbol at code end. */
} > m_data
__CODE_END = __CODE_ROM + (__code_end__ - __code_start__);
/* Custom Section Block that can be used to place data at absolute address. */
/* Use __attribute__((section (".customSection"))) to place data here. */
.customSectionBlock ORIGIN(m_data_2) :
{
KEEP(*(.customSection)) /* Keep section even if not referenced. */
} > m_data_2
/* Uninitialized data section. */
.bss :
{
/* This is used by the startup in order to initialize the .bss section. */
. = ALIGN(4);
__BSS_START = .;
__bss_start__ = .;
*(.bss)
*(.bss*)
*(COMMON)
. = ALIGN(4);
__bss_end__ = .;
__BSS_END = .;
} > m_data_2
.heap :
{
. = ALIGN(8);
__end__ = .;
PROVIDE(end = .);
PROVIDE(_end = .);
PROVIDE(__end = .);
__HeapBase = .;
. += HEAP_SIZE;
__HeapLimit = .;
__heap_limit = .;
} > m_data_2
.stack :
{
. = ALIGN(8);
. += STACK_SIZE;
} > m_data_2
/* Initializes stack on the end of block */
__StackTop = ORIGIN(m_data_2) + LENGTH(m_data_2);
__StackLimit = __StackTop - STACK_SIZE;
PROVIDE(__stack = __StackTop);
.ARM.attributes 0 : { *(.ARM.attributes) }
ASSERT(__StackLimit >= __HeapLimit, "region m_data_2 overflowed with stack and heap")
}
Hello,
this is standard GNU Linker file. You can find many tutorials on Internet - for example Here
Jiri