AnsweredAssumed Answered

i.MX 6q - Nougat - audio codec issue

Question asked by RAVIKIRAN J J on Sep 14, 2017
Latest reply on Oct 31, 2017 by RAVIKIRAN J J

Hi All,

 

 

I am working on the imx6q based customized board  with sgtl5000 audio codec , Nougat porting.

Is it possible to set the codec sampling rate by default to 16K.

 

As of now if i make some  modification in the HAL  :

For less than 32k -- Codec is setting to 32k sampling rate.

For 32K-44k -- Codec is setting to 44100 HZ sampling rate.

For 44K-48 -- Codec is setting to 48000 HZ sampling rate.

 

I want to set the default sampling rate as 16K..

Any suggestion please ??

 

Regards,

Ravikiran

Outcomes