AnsweredAssumed Answered

IMX6Q,3.14.52在SPI发送waitstates是否可以去掉?如图

Question asked by 屠珂楠 屠 on Sep 13, 2017
Latest reply on Sep 13, 2017 by 屠珂楠 屠

发送SPI的时候,如图 

这是时钟频率。2个字节之间有一个2.7微妙左右的时间间隔,我一个字节时间也就4微妙。这样效率太低了。手册上关于这里面的 也有这样的时序图 

 

我读寄存器发现 

这个已经是0 wait states了,不知道这个2.7微妙哪里来的。

我做的是这么一个项目,SPI发送速率1.8m,VPU压缩码率是0.8-1.2m这样,每秒会插入一个10000-20000的I帧,每秒25帧通过SPI发送,会分成每包256字节、所以每次在发送I帧的时候,大概需要100ms。画面会卡顿一下。Can somebody help me? thank you!!

Outcomes