SDIO card enumeration problem on Android marshamallow

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDIO card enumeration problem on Android marshamallow

706 Views
susangracerapak
Contributor II

Hi,

I am working on porting my WIFI driver on Android marshmallow for Sabresd board. I have ported for USB successfully.for SDIO,the enumeration is failed.I have observed that , by default only BCMDHD module can used here.
How to use my own SDIO card ?

Can anyone help me ?

Regards

Susan

0 Kudos
1 Reply

545 Views
igorpadykov
NXP Employee
NXP Employee

Hi Susan

you should obtain driver (compatible with used linux kernel version) from

vendor of custom wifi sdio card and include it in linux image, BCMDHD module

can be removed from image using attached Linux Manual sect.4.12.2.3 Menu Configuration Options.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos