AnsweredAssumed Answered

Problem in CAN Frame Transmission in iMX28 EVk linux 2.6.35

Question asked by Karthikeyan S on Sep 13, 2017
Latest reply on Sep 15, 2017 by Karthikeyan S

Hi,  I am not able to set bitrate using below command, ip link set can0 type can bitrate 125000Instead, I did following command to set the bit rate# echo 125000 > /sys/devices/platform/FlexCAN.0/bitrate But, I am trying send CAN frame using following Commandcansend can1 -i 0x10 0x11 0x22 0x33 0x44 0x55 0x66 0x77 0x88 In Second Board, I was using following command to receive the CAN framecandump can1 But I am not getting anything. Please suggest me to resolve this issue as soon as possible
 

root@mx28evk /sys/devices/platform/FlexCAN.1$ candump can1
interface = can1, family = 29, type = 3, proto = 1

  root@mx28evk /sys/devices/platform/FlexCAN.1$

Outcomes