AnsweredAssumed Answered

P1010 UART controller ETHREI interrupt not pending

Question asked by 航天 刘 on Sep 12, 2017
Latest reply on Oct 10, 2017 by alexander.yakovlev

P10101 board UART ETHREI  interrupt can not pending,which causes data can not be sent out through serial port. P1010 uart uses 8250 uart driver,and i find two known bugs which are fixed through two flags UART_BUG_TXEN and UART_BUG_THRE。 These bugs are similar with the problem I encountered, except that I encounter this problem when the serial is be using normally, but UART_BUG_TXEN and UART_BUG_THRE are detected and set when UART startup。How to handle this problem?The following is the UART register scene when the problem occure:

0x4500 : 0x00

 

0x4501 : 0x07

 

0x4502 : 0xc1

 

0x4503 : 0x13

 

0x4504 : 0x0b

 

0x4505 : 0x60

 

0x4506 : 0x00

 

0x4507 : 0x00

 

0x4508 : 0x00

 

0x4510 : 0x01

 

The ETHREI interrupt is enable,  TEMT and THRE are set, but no interrupt is pending. I need emphasize that i encountered when the serial is be using normally and the two flags "UART_BUG_TXEN and UART_BUG_THRE" is not set.

Outcomes